ค้นหาคำศัพท์

แสดง 1 เป็น 10 ของ 15 ผล
Radial fan กรุนด์ฟอส
A radial fan is a device that consists of an impeller driven by an electrical motor.
Radiant heating กรุนด์ฟอส
Radiant heat is thermal radiation between two surfaces.
Radiator exponent กรุนด์ฟอส
The radiator exponent n indicates the change in heat output of a radiator when the actual conditions, in terms of water temperature and room temperature, differ from standard conditions, i.e., the values that were used to define a radiator’s nominal heating capacity.
Radiator กรุนด์ฟอส
A radiator is a heating surface that transfers a significant part of its heat by thermal radiation and the rest by convection.
Reciprocating compressor กรุนด์ฟอส
Reciprocating compressors are often used in connection with cooling systems.
Recirculation pump กรุนด์ฟอส
The function of the recirculation pump is to ensure that hot water is always available as close to the consumption point as possible, in order to reduce water wastage and to increase comfort.
Recycling กรุนด์ฟอส
Recycling creating new products from used materials. Recycling is not the same as reuse, where the object is reused for its original purpose.
Refrigerant charge กรุนด์ฟอส
Refrigerant charge is a term used for the type and mass of refrigerant a refrigeration plant will hold to perform under the given conditions.
Refrigerant กรุนด์ฟอส
The task of the refrigerant is to transfer energy from one level and dispose of it at a higher level.
Relative humidity กรุนด์ฟอส
Relative air humidity is a term used to describe the amount of water vapour in the air.