ค้นหาคำศัพท์

แสดง 1 เป็น 10 ของ 17 ผล
HCFC (Hydrochlorofluorocarbon) กรุนด์ฟอส
CFC and HCFC refrigerants are detrimental to the breakdown of the ozone layer and the greenhouse effect.
Header กรุนด์ฟอส
A header is a manifold, the purpose of which is to uniformly distribute coolant in pipe circuits in air coolers, dry coolers, evaporators and condensers.
Heat exchanger กรุนด์ฟอส
Heat exchangers are used in heating systems to separate two media, while at the same time transferring heat from one to the other.
Heat pump กรุนด์ฟอส
A heat pump is a system that can both cool, heat, and dehumidify air in a room, depending on the demand.
Heat recovery กรุนด์ฟอส
A great part of energy consumption in a ventilation system goes to heating outside air.
Heat rejection กรุนด์ฟอส
Heat rejection is the excess heat from a cooling system which is removed by the condenser/cooling tower.
Heat requirement กรุนด์ฟอส
A building’s heat requirement need is calculated based on its estimated heat exchange with the surroundings and the building’s users.
Heat transfer fins กรุนด์ฟอส
Fins are used on all air coolers, dry coolers, evaporators and condensers that transfer energy from a liquid media to air or from air to liquid.
Heating surface กรุนด์ฟอส
The heating surface can be an integrated part of the AHU, or be placed directly in the air intake duct.
HFC (Hydrofluorocarbon) กรุนด์ฟอส
HFC as a refrigerant does not contribute to the breakdown of the ozone layer, but contributes to the greenhouse effect.