ค้นหาคำศัพท์

แสดง 21 เป็น 30 ของ 354 ผล
Balance point กรุนด์ฟอส
In any thermal heat exchange process, a mixture of two energy flows will result in a new stage or phase called the balance point.
Balancing valve กรุนด์ฟอส
During commissioning of heating and cooling systems, hydraulic balance is often achieved using balancing valves; static or dynamic.
Balancing กรุนด์ฟอส
Balancing of heating and cooling systems is performed to ensure that the correct amount of water is present at all consumption points.
Biocide กรุนด์ฟอส
Biocide is a chemical added to the make-up water for evaporative applications such as condensers and cooling towers.
Biofilm กรุนด์ฟอส
Biofilm refers to a population of various micro-organisms trapped in a layer of slime and organic matter that attaches itself to the surfaces of pumps, pipes, walls etc.
BMS (Building Management System) กรุนด์ฟอส
A BMS is an integrated data network and control system for automation, monitoring and control of HVAC, lighting and other functions in a building.
BOD (Biochemical Oxygen Demand) กรุนด์ฟอส
The quantity of oxygen consumed by aerobic microorganisms during the decomposition of organic matter in a water sample is defined as the Biochemical Oxygen Demand (BOD).
Boiler shunt กรุนด์ฟอส
The primary task of the boiler shunt is to ensure that the difference in temperature between the top and the bottom of the boiler is not too high. A high temperature difference can cause tensions in the material and thus reduce the life of the boiler.
Boiler กรุนด์ฟอส
Consumers who live in areas with no district heating have to use their own boiler to produce central heating. A boiler installation has the following components: burner, nozzles, boiler casing, hot-water tank (integrated or separate) and a chimney.
Brackish water กรุนด์ฟอส
Brackish water is water that has more salinity than fresh water, but not as much as seawater.